iVu Gen2 - Release Notes (2015R1)

|---------------------------------------------------------------------------|
|--------| This document contains information on current and past  |--------|
|--------| software releases for all iVu (Stardard) Gen2 products. |--------|
|---------------------------------------------------------------------------|

=============================================================================
Current Release - v2.2.0                                         (April 2015)
=============================================================================
*** All iVu (Standard) Gen2 models ***

   Resolved Issues:
   - In some cases, dark and low contrast images with small FOV may show vertical 
     noise lines. 
     
     Note: After installing this firmware, captured images could be up to 3% 
           brighter. Existing inspections might need to be modified.

=============================================================================
Release - v2.1.2                                                (March 2015)
=============================================================================
*** All iVu (Standard) Gen2 models ***

  Resolved Issues:
  - Incorrect imager settings were resulting in some devices to be misidentified
    as failures during the manufacturing process. 

    Note: It is not neccessary to update existing devices; however, if an existing
          device is updated, the new imager settings will not negatively affect
          current inspections.

=============================================================================
Release - v2.1.1                                              (October 2014)
=============================================================================

*** All iVu (Standard) Gen2 models ***

  - Initial release on iVu (Standard) Gen2 hardware.
  - Configurations can be imported to Gen2 models from previous (Gen1 Standard)
    models.

 New Features:
  - Added support for "Fine" and "Coarse" imager resolution.
  - Added capability to mask part of captured image when running Area and 
    Blemish sensor types.
  - NPN/PNP is user selectable. These are no longer separate models.
  - Pull-up resistor is user selectable. External resistor is no longer needed.
  - The TG and BCR firmware files can be loaded into any of its derivative 
    devices as defined below. The firmware will identify the hardware and 
    configure itself for that device's feature set. 
        - TG2_vXXX.BIN can be loaded on the following:
            - iVu TG Gen2 (Integrated Display)
            - iVu RG Gen2 (Remote Display)
            - iVu TG Plus Gen2 (Integrated Display)
            - iVu RG Plus Gen2 (Remote Display)
       - TB2_vXXX.BIN can be loaded on the following:
            - iVu TB Gen2 (Integrated Display)
            - iVu RB Gen2 (Remote Display)
            - iVu TB Plus Gen2 (Integrated Display)
            - iVu RB Plus Gen2 (Remote Display)

=============================================================================
CD Contents:
=============================================================================

    - Emulator Install Program
    - Product Reference Materials
    - Firmware Update Wizard
    - Password Reset Utility
    - Sample Applications and Notes
    - Sample Programs with source code

=============================================================================
Emulator - System Requirements:
=============================================================================

    - Microsoft Windows8, Windows7, Vista, XP.
    - USB Port to import and export files from USB Flash Drive.
    - Typical installation requires 15 megabytes of free disk space.
    - Minimum video display resolution setting is 1024x768 at 256 color.
    - Up to 50 MB of RAM (excluding amount of RAM required by operating 
      system and other applications).
    - Acrobat Reader to read documents.

=============================================================================
BANNER CONTACT INFORMATION
=============================================================================

    Address: Banner Engineering Corp.
             9714 10th Avenue North 
             Minneapolis, MN 55441

      Phone: (763) 544-3164
        Fax: (763) 544-3213
  Toll Free: 1-888-3-SENSOR (1-888-373-6767)
  
    Website: http://www.bannerengineering.com


=============================================================================
All contents (c) 2014 Banner Engineering Corp.